Output Amplitude

You can set the output amplitude in Vpp, Vrms, or dBm.

BenchVue Tip: You can quickly increment or decrement a numeric value using the mouse wheel. Click once in a number entry field and then scroll the mouse wheel up or down.

See Also

To view instrument manuals, click on Library tab from main BenchVue application window.

DC Offset Voltage

Output Load Termination

Output Units